We implemented an efficient logistics concept at Brenntag Schweizerhall AG's Basel site
Chemicals distributor Brenntag Schweizerhall AG provided clear proof of their competence in the area of customer proximity through partnership: The company set up in Infrapark Baselland so that they could supply chemical raw materials directly to the businesses there.
Control cabinet with integrated operating panel
Benefits
Chemical raw materials in the required quantity and concentration "just in time"
Faster and more reliable data exchange thanks to the integration of 9 production buildings in the automation network
Complete delivery and commissioning of the entire automation technology from a single source
"Efficient automation technology is a must in order to deliver chemical raw materials just in time"
Wolfram Heymann, CEO
Brenntag Schweizerhall AG
The customer's requirements
Construction of such plants is no ordinary challenge as working with sulfuric acid, hydrochloric acid and caustic soda requires more stringent safety precautions. Therefore a risk analysis was first commissioned which would serve as the basis for the project. The project also included full automation of all processes. Brenntag Schweizerhall AG chose Endress+Hauser (Schweiz) AG as the supplier for the measurement instrumentation and automation technology.
The Endress+Hauser solution
All aspects of the automation concept had to be implemented. The task was to manage the processes reliably based on the risk analysis carried out and to design the plant in such a way that operation is easy. The plant is operated via 8 local stations as well as from Brenntag Schweizerhall AG's headquarters in Basel.
Water, natural gas, steam, mineral oil, chemicals are some of the fluids that have to be measured every day in. Learn more about flow measurement and select the best flowmeter for your process needs.
Откройте для себя отраслевые решения Endress+Hauser для точного и безопасного коммерческого учета жидких продуктов в автомобильном и железнодорожном транспорте.
Brenntag Schweizerhall AG - швейцарская дочерняя компания Brenntag AG, мирового лидера в дистрибуции химических веществ. В компании работает около 220 человек; специализация компании - нестандартные, клиентоориентированные решения по логистике и обслуживанию.
Ваша конфиденциальность очень важна для нас
Мы используем файлы cookie для повышения удобства просмотра веб-страниц, сбора статистических данных для оптимизации функциональности сайта, а также для показа рекламы и контента, адаптированных специально под вас.
Выбирая опцию "Принять все", вы соглашаетесь с использованием нами файлов cookie.
Для получения более подробной информации ознакомьтесь с нашей Политикой использования файлов cookie .